Thermal interface management (or keeping components cool) is a perennial problem, which is why heat sinks and thermal materials are such a key component in electrical circuits and devices. Fischer Elektronik has been manufacturing products which take the heat off components throughout the company's history. The excellent cooling properties, resistance ranges and compatibility of their products have made Fischer heat sinks some of the most highly regarded in the electronics industry.
Fischer heat sink systems includes aluminium bolt-on and clip-on devices compatible for vertical and horizontal mounting on all industry standard semiconductor packages, such as TO-220, SOT-32, TO-3 and D-PAK. The heatsinks are finished in a black anodised substance which increases radiative cooling, thermal conductivity and maximises heat loss. Fischer heatsinks can be applied to the heat loss of semiconductors, components and PCB configurations such as LEDs, IGBTs, BGAs, CPUs, as well as solid-state relays.
Customers requiring Fischer heat sinks and thermal management accessories for their applications have an extensive range to choose from at Rapid Electronics. These high performance devices, available in a range of sizes, plate thicknesses and characteristics, can be bolted on or clipped on to semiconductors and PCBs, providing differing thermal resistance values suited to particular applications.