Item added to basket:
{{AddedItem.TotalPriceText}}
- {{query}}
- {{suggestions.ScopedQuery}} in {{scope}}
- {{brand.contentName}}
- {{tier.contentName}}
-
Other Suggestions
- {{page.contentName}}
Re-reeling orders placed after 16:30 will be processed the next working day.
These black zip cable ties can be used to hold together and manage cables, band rubber cords, or attach to rollers or tank tread to assist an intake mechanism.
The cable tie consists of a flat section with triangular teeth that slope in one direction, as in a ratchet mechanism. The head of the cable tie has a slot with a flexible pawl that rides up the slope of these teeth when the tape is inserted. Once the pointed tip of the cable tie has been pulled through the case and past the ratchet, it is prevented from being pulled back, the resulting loop may only be pulled tighter.
Type | Cable tie |
---|---|
Height | N/A |
Length | 100mm |
Pack Size | 100 |
Thread | N/A |
Width | 2.5mm |
Available for re-reeling
Re-reeling orders placed after 16:30 will be processed the next working day.
To use this facility please Sign In.
Sign In