STANZA AND STEELE - FUSING ELECTRONICS WITH ART
When we sell 100 units of an OLED display, we are always a little intrigued about what they are being used for. Perhaps something more than a display in a PLC, or an output for a home-made electronics project? So it is always interesting to discover that they have actually helped to create something truly unique.
Ian Steele, who is an expert in electronics, audio and software development, worked with conceptual artist Stanza on ‘The Reader', a six-foot high work of electronic installation art which first went on display in 2015.
The figure in ‘The Reader' is the artist himself, depicted wearing a hoodie and reading a book, but the body is covered with the displays, wired up to Arduinos, showing random live data. What does it represent? In the words of the artist himself, “the sculpture becomes a pulsing algorithmic heartbeat. The artwork explores new ways of thinking about life, the emergence and interaction within public space, and how this affects the socialization of space”.
The idea behind the piece, as Steele explains, is to ‘show how embedded technologies will become part of our everyday lives'.
How did you become involved with 'The Reader'?
"I was approached by Stanza after he was commissioned to create ideas for some pieces to be shown as part of an exhibition in Milton Keynes Library". While Stanza worked on the Perspex structure, which was put together in blocks created from a 3D scan of the artist's body, Steele developed the electronics. "I used 100 OLED displays bought from Rapid to visualize the data. The data comes from a large database of books from the British Library. It was important to make the wires and control boards part of the piece. I used six Arduino Mega boards as nodes that control 16 displays. I wrote a custom app for Mac OSX that reads and processes the data and sends it to the display nodes. It also incorporates L-wire and flexi LED strips".
The sculpture is currently working its way through reading all the books published since 1952 via a British Library open source data set. But the work can be adapted and customised to read stock exchange data, DNA data, live news and social media feeds.
What brought Stanza and Steele together? "I have worked with Stanza for about 10 years", says Steele. "I saw some of his work at the ICA in London and have worked on various projects over the years. My strength is in working out the technical processes to realise an artistic concept and I like the mixture of art, software and hardware".