Kingbright is a world-leading manufacturer of LEDs and optoelectronic components. Rapid has been an official distributor of Kingbright LEDs for more than 30 years, and offer a comprehensive service for customers wishing to buy Kingbright products.
As one of Kingbright's leading UK distributors, Rapid can offer excellent rates on high volume orders. The full Kingbright range available from Rapid include displays, surface mount LEDs, 3mm, 5mm, 8mm and 10mm LEDs, light bars and bargraphs, miniature, rectangular, power LEDs, indicators, optics and mounts, clusters, photodetectors, photocouplers, infrared devices and strips.
Founded in Taipei, Taiwan in 1980, Kingbright are at the cutting edge of the fast moving solid state lighting sector. There is huge global demand for Kingbright LEDs and related products, and Kingbright constantly strive to meet the designs and demands of their customers, which include international manufacturers of home appliances, security systems, telecommunications equipment, computers and automotive products.
"The long relationship between Kingbright and Rapid has been critical to the success of Kingbright in the marketplace", says W. J. Song, President of Kingbright Electronics. "This cooperation is built on the fundamental principles of Innovation, Quality, Efficiency and First Class Service, which are shared by both companies and drive our mutual success".
Whatever Kingbright LED you require - even if we do not hold current stock at Rapid - we can source it on short lead times. This is due to our excellent relationship with the manufacturer. Rapid hold stock of a high volume of Kingbright lines and with stock arriving regularly, we can provide access to the entire Kingbright portfolio. We can also work with customers on new designs: helping you through the design process with product samples, and offering support with your production, from small volumes all the way through to full scale production.
Unfortunately re-reeling is not available at the present time for this item as the required quantity is greater than the available stock.
Re-reeling orders placed after 16:30 will be processed the next working day.
Unfortunately re-reeling is not available at the present time for this item.
Price per unit {{ IncVat ? 'Inc' : 'Ex' }} VAT
This product will not be replenished, however, you may buy the remaining stock.
Order in multiples of {{product.InMultiple < product.MinSalesQty ? product.InMultiple : product.MinSalesQty}}
Order in multiples of {{product.InMultiple < product.MinSalesQty ? product.InMultiple : product.MinSalesQty}}
Quantities over {{ product.ReReel.MaxReelSize }} will be supplied on multiple reels.