Industry Schools FE/HE Site: Industry Site: Schools Site: FE/HE Site: Mobile
+44 (0)1206 751166

      Suggested Queries


RasPiO® Duino Arduino Compatible Add on Board for the Raspberry Pi 3, 3B+ & Zero

Order Code:  

75-0902

  Copy to clipboard
Brand: RasPiO  Copy to clipboard MPN: Duino Copy to clipboard
 Report an error
Qty Unit Price (Ex VAT)
1+ £2.28

Get a quote for large quantities here

Price per unit {{ IncVat ? 'Inc' : 'Ex' }} VAT
Contact us for lead times on larger quantities
1 in Stock, despatched same dayContact us for additional stock
The RasPiO Duino is a small plug-on board that has functionality similar to that of an Arduino, but is programmable from the Raspberry Pi. Once it has been programmed it can be removed from the Pi and used on its own, or can be used interactively with the Pi. There is a 72-point prototyping area and the Pi's GPIO ports are also broken out onto the Duino.

All the ports on the Duino are clearly labelled. Each of the useful pins on the ATmega are broken out to a cluster of three holes. Male and female headers are provided, so you can connect whatever you like to your RasPiO Duino.

The Duino comes as a kit and will take about 30 minutes to build, with some soldering required. Once you have built it, software programming should take another 15 minutes and then you are ready to go. For programming, there are three jumpers to connect the microcontroller’s SCLK, MISO and MOSI directly to the Pi’s corresponding pins. For two-way serial communication with the Pi, if you need it, you can add two more jumpers to connect the Pi and ATmega’s Rx and Tx serial ports. RasPiO Duino uses the ATmega 328P-PU which is the same microcontroller chip as both Arduino Uno and Gertboard. It has a 6 channel analog to digital converter (ADC) and 14 digital I/O pins, 6 of which can also be used for PWM.

To make things easier, and to get lots of information on the Duino an excellent full user guide and Arduino programming instruction manual has been produced:

"Learn Arduino Programming with RasPiO Duino"

This book contains all the information you need to get into Arduino programming on the pi, such as:

Brief technical information
A brief build guide (with links to in-depth assembly instructions)
Comprehensive software installation instructions
Lots of example sketches and walk-throughs showing how to use the capabilities of the board
Links to the RasPiO Duino github repository
An easy-install script for the sketches
High-quality diagrams and photographs
47 Pages of educational inspiration, discovery and fun
  • Low cost, easy introduction to Arduino programming on the Raspberry Pi
  • For beginners and more advanced users
  • Supplied as a kit (some soldering required)
  • Runs on 3V3 12MHz

You can download the programming manual here

For instructions on assembling the kit see here.

There are video tutorials to help you learn programming, see here.



Type Duino Arduino programming on Raspberry Pi

To use this facility please Sign In.

Sign In

Reviews


Be the first to submit a review