Item added to basket:
{{AddedItem.TotalPriceText}}
- {{query}}
- {{suggestions.ScopedQuery}} in {{scope}}
- {{brand.contentName}}
- {{tier.contentName}}
-
Other Suggestions
- {{page.contentName}}
Dash and Dot apps are available on iOS, Android and Kindle. Download them for free via your devices app store. Please note that Go! is not available on Kindle.
This app is for your youngest kids from reception class upwards.
Go! acts as a remote control for Dash robot.
What is Go! good for?
Xylo is designed to be used specifically with the Dash Xylophone accessory. This accessory is available separately or is included as part of the Wonder Pack. Xylo introduces children to both programming and music by allowing them to create visual sequences of notes which Dash can then play on the Xylophone.
What is Xylo good for?
Path allows you to draw a route for the Dash robot to follow. When you press the head of the on-screen Dash, the real-life Dash robot will follow the path you have drawn. You can drop various icons along the way, so that the robot plays a sound or does an action at certain points along the route.
There are various "challenges" within the software such as a racetrack and farmyard but perhaps the most powerful part is the free space which allows children to explore distances, estimating, sequencing and more.
What is Path good for?
Wonder is an introduction to coding which lets children discover sequences and algorithms using a very visual interface. Connect the commands together with lines much like you would with a flow chart and use inputs from sensors to control the program flow.
For children that are completely new to coding, Wonder can be easier to understand than the more traditional Blockly language.
What is it good for?
Blockly is the full programming app for the Dash robot and Dot robot - it's ideal for teaching coding and can be used in conjunction with the accessories like the launcher and the pen add on to create exciting tasks It can also be used with the Challenge Card Set and the Learn to Code Curriculum Guide teacher book which sets mini-challenges for students to solve and give the teachers solutions explanations.
What is it good for?